DUG_PowerTagE_WSE-04

Enabling Personalized Energy Insights

Using the Wiser app you can enable Personalized Energy Insights to monitor the energy breakdown, and comparison between similar homes and also view energy-saving tips.
IMPORTANT: To enable Personalized Energy Insights you must meet the following conditions:
  • User should be registered in the Europe data center.

  • Users home location must be Sweden/Finland.

  • One PowerTag should be configured as Grid (main incomer).

To enable Personalized Energy Insights:

  1. On the Home page, tap Energy Dashboard > Insights, then tap splash screen (A).

    NOTE: Do not accidentally close the splash screen as it takes 3 weeks for this option to reappear, until that you cannot enable to Personalized Energy Insights.
  2. Read the tutorial information and tap Next twice, then tap Unlock Personalized Energy Insights.
  3. Read the privacy notice and tap Activate on each page.
    NOTE: Accepting consent is optional.
  4. Once Personalized Energy Insights is successfully enabled, you will receive an in-app notification and then immediately you will be prompted to create a home profile. Refer Creating home profile.
    NOTE: You can also navigate through in-app notification which is received after enabling Personalized Energy Insights by tapping .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?