DUG_PowerTagE_WSE-04

Identifying the device

Using the Wiser app, you can identify the PowerTag.
  1. On the Home page, select the desired equipment PowerTag from the list of available devices.
  2. Tap Settings and then tap Identify (A).

  3. Tap OK on the pop-up notification panel when the PowerTag is identified.
    NOTE: The green LED on the identified PowerTag blinks for 30 s.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?