DUG_PowerTagE_WSE-04

History

Using the Wiser app, you can monitor the energy consumption by accessing the history.

History of energy consumption:

To view the overall energy consumption.

  1. On Home page, tap Energy Dashboard > History.

  2. On the History page, select a required time frame (A):

    • Hours: to view the hourly consumption.

    • Days: to view the daily consumption.

    • Months: to view the monthly consumption.

    • Years: to view the yearly consumption.

    NOTE: (B) indicates the missing data for a specific duration, when the PowerTag was offline/disconnected.


    NOTE: Tap on the required hour/day/month/year in the bar graph to view the energy consumption.

History of load consumption:

To view the breakdown of energy consumption based on loads.

NOTE: Users with multiple PowerTag configurations or who have enabled Personalized Energy Insights can view the history of load consumption.

  1. On the History page, tap and select Load consumption.

  2. Tap (A) and select a required time frame:

    • Hours: to view the hourly consumption.

    • Days: to view the daily consumption.

    • Months: to view the monthly consumption.

    • Years: to view the yearly consumption.


    TIP: Select the desired load, for example Lighting, Heating etc. to view the load consumption data.
    NOTE: Select the required hour/day/month/year in the bar graph to view the respective breakdown.
  3. Tap toggle switch (B), for a breakdown of measured and estimated load consumption.

    NOTE:
    • Measured and estimated load consumption feature is available only for Personalized Energy Insights users.
      For other users by default measured values will be displayed.

    • It is only possible to enable this feature for months and years breakdown.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?