DUG_PowerTagE_WSE-04

Checking currency type

You can view the currency type in the Wiser app.
NOTE: Default currency is set based on the home location.
To view currency type:
  1. Tap on the home page.
  2. Select Home Management and select your home where the energy device is installed, to view Home Settings.
  3. On Home Settings page, you can view the currency type.
    Following currency are available based on home location:
    • Kr NOK: Norway

    • Kr SEK: Sweden

    • Kr DKK: Denmark

    • € EUR: Finland and Spain

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?