DUG_PowerTagE_WSE-04

Removing the device

Using the Wiser app, you can remove a device from the device list.
To remove a PowerTag:
  1. On the Home page, tap All devices and select the PowerTag to be removed.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A) > Confirm.
    TIP: On the Home page, tap and hold the PowerTag to remove the device.
    All the historical data will be deleted in the app and cloud.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?