DUG_PowerTagE_WSE-04

Insights

Using the Wiser app, you can check the annual bill for a specific tariff for all users.
Similar home energy comparision and energy saving tips for Personalized Energy Insights users.
  1. On Home page, tap Energy Dashboard > Insights.
  2. On the Insights page, you can see the following:
    • Annual bill as per the tariff set (A) (for all user).

    • Comparision of energy consumption with similar homes and energy saving tips (for Personalized Energy Insights user only).

      • (B) indicates energy consumption of your home.

      • (C) indicates energy consumption of similar homes.

      • Update home profile (D).

      • Energy saving tips (E).

      • List of additional tips to save energy (F).

  3. Tap (F), to View all tips.
    • To Do (G): list of tips to save energy.
    • Done (H): list of completed tips.
    TIP:
    • Tap on Read more to view the detailed information regarding the tip and also the estimated savings per year.

    • Once the tip on To Do tab has been implemented, tap Mark As Done. The tip will now appear in Done (H) tab.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?