DUG_Exxact – rums-/golvtemostat 16 A_WH-00

Creating a moment

A Moment allows you to group multiple actions that are usually performed together. By using the Wiser Home app, you can create moments based on your needs.
To create a moment:
  1. On the Home screen, tap .
  2. Go to Moments > to create a moment.
  3. Enter the name of the moment (A).
    FÖRSLAG: You can choose the cover image that best represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. In the Add actions menu, you can select the devices (C).
  6. Once all the device are selected, tap Done.
  7. On the Moment creator page, tap the device to set the condition. For example, select heating.
    • Set the required temperature using sliding bar (D).

    When the desired condition is set, tap Set.

  8. Once all conditions are set, tap Save.
Once the moment is saved, it is visible on the Moments tab. You can tap on the moment to enable it.
FÖRSLAG:
  • If you want to see the created moments on the Home screen, go to Home > > Home screen > Moments. Enable the toggle button to view moments on the Home screen.

  • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Var det här till hjälp?