Device control
You can control a Device in your Home directly on the Control tab for quick control or in the Device Control Screen.
Control tab
On the Control tab, you can find all the devices installed in your home. The devices are arranged according to the Rooms they are assigned to, making it easy to manage and control them.
Detailed information about setting up Climate devices can be found in chapter Climate control.
-
Tap on the icon (A) available under each device to quickly control a device (e.g., turn it on/off, adjust the temperature or adjust the shutter).
Device Control Screen
The advanced controls such as device settings or creating/assigning schedules will be performed in the Device Control Screen.
-
On the
, tap the device (A) you want to control. -
Set the desired state/value for the Device.
Device Control screen:
B |
Tap to manually turn the device on or off. The green icon indicates the device is currently ON. |
C |
Enable/disable to follow the pre-set schedule for the device. If the schedule is not yet created for the device, a Create or assign a scheduleoption will be available to create a new schedule or assign the device to an existing schedule. Refer to Schedule for detailed information. |
D |
Redirects you to Schedule details screen to modify your existing schedule. Refer to Editing a Schedule. |
E |
Navigates to the Device Details |