System User Guide Wiser Home (Germany, Austria) - 14

Safety and Security

Wiser Smoke Alarm - Battery

CCT599002

Detects smoke and fires.

Instruction Sheet

Device User Guide

Wiser Window/Door Sensor

CCT591012

Can be used to detect if a door or window is opened or closed.

Instruction Sheet (PDF)

Device User Guide

Wiser Motion Sensor

CCT595012

Reports the detection of movement and measures the luminance of the environment.

Instruction Sheet (PDF)

Device User Guide

Wiser Water Leakage Sensor

CCT592012

Detects water on a surface.

Instruction Sheet (PDF)

Device User Guide

Wiser Temperature/Humidity Sensor

CCT593012

Measures temperature and humidity

Instruction Sheet (PDF)

Device User Guide

ARGUS Outdoor Motion Sensor 360

MEG5641–3119
MEG5641–3114

It offers advanced motion detection, LUX measurement, and temperature sensing capabilities. It allows you to automate and enhance your smart home environment effortlessly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?