System User Guide Wiser Home (Germany, Austria) - 14

Creating a Moment

On the Automation screen:

  1. Tap icon to navigate to moment creator screen.

  2. Select an icon from the list (A).

  3. Enter a name for the Moment into the text field. (B).

  4. Tap Add actions (C).

  5. Tap the Device you want to add to the Moment.

    TIP:
    • Tap a selected Device again to remove it from the Moment.

    • You can add any device from your home to create a moment. The maximum number of devices you can add to a moment is 60.

  6. Tap Done.

  7. Tap a Device to open the Device Control and set the state you want to put the device into and tap Set in the upper right corner.

    Repeat for all devices.

  8. Tap Save.

    TIP: You can remove a Device by swiping it left and taping the icon.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.