System User Guide Wiser Home (Germany, Austria) - 14

Appliances

Connected Single Socket Outlet 16A

MEG2380–0xxx

Remotely control and monitor the power consumption of the plugged-in load.

Instruction Sheet (PDF)

Device User Guide

Wiser Power Micromodule

CCTFR6730

The Wiser Power Micromodule is for switching loads (up to 3000 W resistive) such as a hot water tank or a socket outlet.

In combination with the Wiser app, the energy consumption can be measured and the module can be used for load shedding or demand response.

Instruction Sheet (PDF)

Device User Guide

Wiser Plug

CCTFR6501

Remotely control and monitor the power consumption of the plugged-in load.

Connected Wireless Switch 1-gang/2-gang

MEG5001–0300

MEG5001–6000

Battery powered push-button switch.

Buttons can be freely assigned with functions with the Wiser Home App.

Instruction Sheet (PDF)

Device User Guide

Wiser SmartPlug 16 A

CCT711119

Controls various electrical devices, for example floor lamps, radios, ventilators or coffee machines, using the app. Monitor energy consumption of plugged-in devices.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?