System User Guide Wiser Home (Germany, Austria) - 14

Climate

Wiser Radiator Thermostat 2nd Generation

CCTFR6110

CCTFR6111

CCTFR6918 (3 x CCTFR6110)

The Wiser Radiator Thermostat 2nd Generation uses integrated temperature sensors to control the flow of water through a radiator, thereby regulating the temperature in a room. The target temperature and switching times are set in the Wiser Home App.

Instruction Sheet (PDF)

Device User Guide

Wiser Radiator Thermostat

CCTFR6100
CCTFR6101

Provides individual temperature control for radiators.

Instruction Sheet (PDF)

Device User Guide

Wiser Room Thermostat with display

CCTFR6400
CCTFR6401

Wireless, battery-powered, colored touch-button display to set the room temperature.

Wiser 16 A Relay for Temperature Control

CCTFR6700

Control electrical heaters with On/Off commands (Relay output) or Fil Pilote commands.

Wiser Underfloor Heating Connection Strip

CCTFR6600
CCTFR6610
CCTFR6620

Control thermal actuator valve heads to regulate the flow of hot water in the underfloor pipes.

Instruction Sheet (PDF)

Device User Guide

Connected Thermostat Module, ZB

MEG5779-0xxx

MEG5779-60xx

See the current room temperature, set the desired temperature and activate boost mode.

To be completed with a Connected Thermostat Insert.

Instruction Sheet

Device User Guide (With 2A Insert)

Device User Guide (With 16A Insert)

Connected Thermostat Insert 2 A

MEG5777-0000

Control water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

To be completed with the Connected Thermostat Module.

Connected Thermostat Insert 16 A

MEG5777-0001

Controls water-based heating and cooling applications, such as electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water based heating.

To be completed with the Connected Thermostat Module.

Instruction Sheet

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.