System User Guide Wiser Home (Germany, Austria) - 14

Editing a Moment

On the Automation screen:

  1. Tap icon.

You can:

  • Change the Icon (A).

  • Change the name (B).

  • Tap the Device to open the Device Control screen (C) and change the state of the device.

  • Tap the Add actions (D) and more Devices to the Moment.

  • Swipe the Device left and tap the (E) to remove a device from the Moment

Tap Save(F) to save the changes to the Moment

.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.