System User Guide Wiser Home (Germany, Austria) - 14

Enabling Wiser Home AI

The following is an example of enabling Wiser Home AI with EV Charger and Water heater installed.

To enable Wiser Home AI:

  1. On the Home screen, tap .

  2. Tap on the banner (A), then tap Try Wiser Home AI.

    NOTE: This feature is currently available as a free preview. It may become a paid feature in the future.

    TIP:
    • Tap (B) to understand more about the feature.

    • Tap (C) to read the terms and conditions.

  3. Tap Optimise your Home Profile > Continue to provide your daily schedule details and set up your profile.

  4. Set the time when you want your car to be charged:

    1. Tap (E), select a time period (F) and tap Set.

    2. Tap (G), select a time period (F) and tap Set.

  5. Tap Next.

  6. Enter the number of kilometers required to drive this car using the dial pad:

    1. Tap On week day

    2. Tap Over the entire weekend

  7. Tap Next.

    NOTE:
    • If you have any one of the supported devices commissioned, you will see only the related questions.

    • If you have all the supported devices commissioned, you will see all questions related to the devices. Example, if you have both EV Charger and Water Heater, you will see further questions for Water Heater.

  8. Enter how many members take showers using the dial pad:

    1. Tap In the mornings

    2. Tap In the evenings

  9. Tap Manage Wiser Home AI.

    You will be directed to Manage Wiser Home AI screen from the > Energy Management > Wiser Home AI to view the devices that are enabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.