System User Guide Wiser Home (Germany, Austria) - 14

Device control

You can control a Device in your Home directly on the Control tab for quick control or in the Device Control Screen.

Control tab

On the Control tab, you can find all the devices installed in your home. The devices are arranged according to the Rooms they are assigned to, making it easy to manage and control them.

NOTE: If you have only one device installed at your home, the Control tab will not be available. You can control the device from the Home screen under Your device or from the Device Control Screen.
IMPORTANT: Climate devices, like Radiator Thermostats, will be controlled like any other Device, but need to be set up properly.

Detailed information about setting up Climate devices can be found in chapter Climate control.

  1. On the Home screen, tap Control tab.

    NOTE: You can also set your Control tab as your default landing screen. To do this, go to > Home Screen and enable the Start on the Control Tab toggle switch.

    A

    Quickly control a device (e.g., turn it on/off, adjust the temperature, or adjust the shutter)

    B

    Indicates that the device is offline. Tap the device to open troubleshooting steps. Tap Learn more to know more about the zigbee signal strength or rap Help & Support if you require further assistance and visit the Wiser Support pages.

    C

    Navigate to the settings screen.

    D

    Add new devices.

Device Control Screen

The advanced controls such as device settings or creating/assigning schedules will be performed in the Device Control Screen.

  1. On the Home Screen > Control, tap the device (A) you want to control.

  2. Set the desired state/value for the Device.

Device Control screen:

NOTE: The options and functions available on the device control screen vary depending on the type of device. For detailed information, refer to the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.

B

Tap to manually turn the device on or off. The green icon indicates the device is currently On.

C

If the device is currently following the schedule, it shows until when the current status will remain active based on the schedule.

For example, here until 14:00 means that device will stay On until 4:00 PM.

D

Enable/disable to follow the pre-set schedule for the device. If the schedule is not yet created for the device, a Create or assign a schedule option will be available to create a new schedule or assign the device to an existing schedule. Refer to Schedule for detailed information.

E

Redirects you to Schedule details screen to modify your existing schedule. Refer to Editing a Schedule.

F

Add or remove the device from Favourite devices. Refer to Managing Favourites.

G

Navigates to the Device Details.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.