Creating an Account
Once the professional installer sets up the Wiser system, they will hand it over to the homeowner. Subsequently, the homeowner will create an account to have control over the Wiser system. Refer to the chapter Setting-up the Wiser System for information on how to setup the wiser system.
If the homeowner decides to set up the Wiser system independently, they need to begin by creating an account before proceeding with setting up the Wiser system.
- On the welcome screen, tap Get started (A).
- Tap Home Owner (B) to create an account.
- Enter your name and e-mail address
- Enter a passwordNOTE: The password must meet at least the following criteria:
-
Eight characters long
-
Contain at least one uppercase and one lower case letter
-
Contain at least one number
TIP: Increase the security of your password by observing the following points:-
Do not use any personal information such as a name, birthday, e-mail address, etc. These data are publicly visible and make it easier to guess the password.
-
Use a long password. It should contain at least six characters; longer passwords help increase security.
-
Do not use a password that you have already assigned for another service.
-
If possible, include numbers, special characters and differences in upper and lower case.
-
Change the password frequently.
TIP: For more information about securing your network, read chapter Cybersecurity Principles -
- Select the country in which your home is located.
- Tap Continue .
- Activate account.An e-mail will be sent to the specified e-mail address. Check your inbox and click the link in the e-mail.TIP: If you do not see the e-mail in your inbox, also check the spam folder if your provider offers one.
You can change the information and have the e-mail sent again
After confirming the e-mail, the Wiser Home app shows the confirmation that the setup is complete.
- Tap
icon.
- Read and tick the check box to agree with the User Agreement and Privacy Notice and tap I accept.
- Personalize your consents and tap Continue.
- Enter your home address and tap Continue.The home address is required so that functions dependent on the location (e.g. Eco-Mode) work properly.