DUG_Underfloor Heating Connection Strip_WH-07

Identifying the device

Using the Wiser Home app, you can identify the Underfloor Heating from the other available devices in the room.
To identify the Underfloor Heating:
  1. On the Home screen, tap .
  2. Tap Devices > Underfloor Heating > Identify (A) to rename the Underfloor Heating.
    NOTE:
    • This feature flashes the Underfloor Heating LEDs, so you can identify the actual device.

    • The Underfloor Heating LEDs will continue to flash until you tap OK.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?