DUG_Underfloor Heating Connection Strip_WH-07

Setting floor sensor limit

Using the Wiser Home app, you can set the floor sensor limit for Underfloor Heating.
  1. On the Home screen, tap .
  2. Tap Devices > Underfloor Heating
  3. Select the following:
    • Floor Sensor Upper Limit: to set upper temperature limit of the floor sensor.
    • Floor Sensor Lower Limit: to set lower temperature limit of the floor sensor.
    NOTE:
    • Floor sensor upper limit temperature should be higher than lower limit temperature.

    • Floor sensor lower limit temperature should be lower than upper limit temperature.

    • The UFH setpoint temperature ranges from 18 °C to 30 °C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?