DUG_Underfloor Heating Connection Strip_WH-07

About the device

The Wiser Underfloor Heating Controller / Connection Strip (hereinafter called Underfloor Heating / UFH) is used to control thermal actuator valve heads to regulate the flow of hot water in the underfloor pipes.

The UFH is available in the following versions:

  • UFH Heat/Cool

  • UFH Heat

  • UFH Heat/Cool 24 V

The UFH Heat/Cool and UFH Heat/Cool 24 V can also be used to control a heat pump or a boiler. The UFH should only be used with hydronic UFH systems. It works in conjunction with the Wiser Hub and Wiser room thermostats, and it controls the temperature for individual rooms/zones.

TIP: There are total 6 channels available on Underfloor Heating, based on your rooms/zones requirement select the channel:
  • 1/2 channel: you can use it for a large room to control 4 thermal actuators valve heads to supply hot water.

  • 3/4 channel: you can use it for a medium room to control 2 thermal actuators valve heads to supply hot water.

  • 5/6 channel: you can use it for a small room to control a thermal actuator valve head to supply hot water.

With mixed systems (UFH and radiators) Wiser radiator thermostats can be added, and in this way a complete hydronic heating system can be controlled. The system is simple to expand: 2 further Wiser Connection Strips (and optionally radiator thermostats) can be added.
1x UFH max. 6 rooms/zones
2x UFH max. 12 rooms/zones
3x UFH max. 16 rooms/zones


Features of the Underfloor Heating:

  • Remotely control Underfloor Heating using the Wiser Home app.

  • Boost the room temperature using the Wiser Room Thermostat center button.

Diagram of operating elements

  1. Setup button

  2. Setup LED

  3. Channel button

  4. Cooling LED

  5. Room names

  6. Channel LEDs 1 to 6

  7. LED for pump contact

  8. LED for burner or boiler

  9. LED for 230 V / 24 V power supply

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.