DUG_Underfloor Heating Connection Strip_WH-07

Installing the device

Refer to the installation instruction supplied with this product.

The following items are needed to install a Wiser UFH system:

  • Wiser UFH Connection Strip/s

  • Wiser Hub or HubR

  • Wiser room thermostat or Wiser Temperature/Humidity Sensor

NOTE:
  • The system can be installed without connecting to a Wi-Fi router.

  • When using UFH Heat/Cool 24 V version make sure it is connected to a 24 V 2.2 A power supply (not included)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?