DUG_Underfloor Heating Connection Strip_WH-07

LED indications

Normal use

LED

LED status

Behaviour

LED

Power plant under voltage

Channel 1‑6 LEDs

off

Relay open (no call for heat)

closed (call for heat)

dimmy lit

Delay in relay activation

System test / emergency heating

Configuration LED

Connected to the Wiser Hub

Attempting to link with the Wiser Hub

No connection with the Wiser Hub

Blinking red

Floor temperature exceeded

LED of a channel

Channels activated

Heating / cooling LED

Cooling mode

Dew sensor activated

Pump LED

Pump activated

Boiler LED

Boiler activated

Settings

User action

LED

LED status

Behaviour

Connection of the control unit for configuration LED from hydraulic floor to the Wiser Hub.

Press and hold the configuration button for more than 2 s.

valves

Turn signal

/

The link is implemented. Follow the instructions of the application.

Resetting the control unit for hydraulic floor valves.

Press and hold the configuration button for more than 20 s.

Configuration LED

Red until that all LEDs are flashing


The control unit for hydraulic floor will be removed from the Wiser platform.

Identification of the control unit for valves. All the hydraulic floor LEDs from the application.

 

Identification

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?