DUG_Underfloor Heating Connection Strip_WH-07

Assigning a channel to the room

Using the Wiser Home app, you can assign Underfloor Heating channel to the room to control the temperature.
Select one or several channels based on your room size or the number of thermal actuators fitted (such as for a small room: channel 5 or 6, a large room: channel 1 or 2).
  • Channels 1 and 2 can be fitted with 4x thermal actuators each.

  • Channels 3 and 4 can be fitted with 2x thermal actuators each.

  • Channels 5 and 6 can be fitted with 1x thermal actuator each.

  1. On the Home screen, tap .

  2. Tap Devices > Underfloor Heating

  3. Tap Channel configuration and select the Channel for which you want to assign a room.

  4. Select a existing room from the list or enter New room name then tap Submit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?