DUG_Iconic Fan controller_WHP-01

About the device

Iconic Connected AC Fan Speed Controller, Zigbee (hereinafter referred to as fan controller) can control up to two fans and in three steps, you can adjust the fan speed to achieve your desired comfort. You can also control the fan using Wiser Home app.

Operating elements

  1. Push-button

  2. Status LED (Amber, Green, and Red LED)

  3. Speed indicating LEDs



NOTE:
  • The LED position will change when the fan controller is installed in a different orientation. To maintain same LED position with change in orientation, refer to the position settings.

  • For information on LED during each control stage, refer LED indication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?