DUG_Iconic Fan controller_WHP-01

Editing a moment

  1. From the Home page, navigate to Automations page.
  2. On the Automations page, tap Moments.
  3. Select the moment you want to edit and tap .
  4. On the Moment editor page, you can perform the following changes:
    • Change the icon .

    • Rename the moment.

    • Tap each action to change the settings.

      • To remove an action, slide the action to the left and then tap (A) to delete it.

      • Tap ⊕ Add actions (B) to add a new action.

  5. Tap Save to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?