DUG_Iconic Fan controller_WHP-01

Editing a schedule

You can edit a schedule using the Wiser Home app.
To edit a schedule:
  1. On the Home page, tap All > Ceiling Fan. .
    TIP: You can also navigate to Automations > Schedules and select a schedule you want to edit.
    NOTE: Tap the Follow schedule toggle switch to enable/disable the schedule.
  2. Tap Edit schedules (A).
  3. Tap SCHEDULE DETAILS and edit the following options:
    • Name (B): You can rename the schedule.

    • Applies to (C): You have an option to select or deselect the device.

  4. Tap EVENTS (D) and edit the events STATE (Fan speed Off/Low/Medium/High) and WHEN (Sunrise/Sunset or specific time range).
    NOTE: You can create a new event by tapping +.
  5. Tap Set to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?