DUG_Iconic Fan controller_WHP-01

Creating an automation

To create an automation:
  1. From the Home page, navigate to Automations page.
  2. On the Automations page, tap Automations.
  3. On the bottom right corner of the screen, tap +.
  4. Tap and choose an icon that best represents your automation.
  5. Enter a name of the automation (A) and select any of the following conditions to trigger an automation.
    • All conditions: All conditions must be met to trigger an automation.
    • Any condition: Any one of the condition must be met to trigger an automation.
  6. Tap Add conditions (B) and select any of the following options (C):
    • Device status change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor.
    • Away Mode (Enable or Disable): The Away Mode is intended to set your Home to a practical state for longer absences, such as leaving for the weekend.
      The fan controller will be off if it is in away mode and enabled.
    NOTE: Maximum 10 conditions can be added.
  7. Select a device to set the condition. Then, choose the state of the device that will trigger the automation, such as the On/Off state or speed level of a fan controller.
  8. Tap Set on the upper right corner of the screen.
    TIP: If you want to change the condition, swipe it to the left and tap the bin icon. Then add a new condition with the required parameters.
  9. To start your automation at a particular time, tap When > Add time and select any of the following options (D):
    NOTE: Maximum 10 time entries can be added.
    • Specific time of day: The automation will trigger at a specific time of the day, such as at sunrise, sunset, or at 8:00 AM.
    • Period of time: The automation will be trigger during time periods such as from sunrise to sunset, from sunset to sunrise, or from 8:00 AM to 5:00 PM.
  10. To add an action, tap Then > Add an action and select any of the following options (E):
    NOTE: Maximum 10 actions can be added.
    • Control a device: Select the device and set the desired state of the device.
    • Send notification: You will be notified if the condition is met.
    • Activate a moment: Select a moment.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
    1. In this example, we will select for Control a device and choose Blind Control switch (F) as the device to trigger an action.
    2. Set the state, such as turning the blind control switch On/Off . Then, tap Set on the top right corner of the screen.
  11. Tap Save.
    The saved automation is displayed on the Automation page. Tap the toggle switch (G) on the Automation page to enable/disable the automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?