DUG_Iconic Fan controller_WHP-01

Creating a moment

You can create a moment using the Wiser Home app.
To create a moment:
  1. From the Home page, navigate to Automations page.
  2. On the Automations page, tap Moments.
  3. On the bottom right corner, tap + to create a moment.
  4. Enter the name of the moment (A).
    NOTE: You can choose the cover image that represents your moment by tapping .
  5. Tap Add actions (B) to select the list of devices.
  6. From the Add actions menu, you can select the devices (C).
  7. Once all the device are selected, tap Done.
  8. On the Moment creator page, tap on the device to set the action:
    • Select the device status or fan speed (D) and tap Set on the upper right corner.

  9. Once all conditions are set, tap Save.
    Once the moment is saved, it is visible on the Moments tab. You can tap on the moment to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?