DUG_Iconic Fan controller_WHP-01

Editing an automation

  1. From the Home page, navigate to Automations page.
  2. On the Automations page, tap Automations.
  3. Select the automation you want to edit.
  4. On the Edit automation page, you can perform the following changes:
    • Change the icon .

    • Rename the automation.

    • Tap each condition to change the settings.

      • To remove a condition, slide the condition towards left and then tap (A) to delete it.

      • Tap ⊕ Add conditions (B) to add a new condition.

    • To change the order of actions, tap the Then option, and hold an action then drag and drop to the desired position.

  5. Tap Save to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?