DUG_Iconic Fan controller_WHP-01

Pairing the device

You can pair a device using the Wiser Home app.
To pair the device:
  1. On the Home page, tap Settings .
  2. Tap Devices.
    The Devices page appears.
  3. On the bottom right corner of the screen, tap +.
    The Add Devices page appears.
  4. Tap the Appliances tab.
    TIP: You can also select a device from the All tab.
  5. Tap Iconic Fan Controller (A) > Done (B).
    The Iconic Fan Controller Setup page appears.
  6. Tap Next.
    NOTE: Make sure your fan controller is wired and powered before proceeding.
  7. Press and hold the push-button for > 8 s to enter pairing mode.
  8. Wait for a few seconds until the LED turns amber. You can also see in the app that the device is joined.
    NOTE: If the LED is not blinking amber, see the instructions by tapping the link LED not blinking amber? or refer to resetting the device manually.
  9. Enter the device name in the Name (C) field.
    NOTE: The Next (D) button will be enabled after entering a name in the name field.
  10. Tap Next (D).
  11. Select the desired location of the device.
    NOTE:
    • If you have not created any rooms, enter the room name in the Name (E) field.

    • The Submit (F) button will be enabled after selecting a desired location.

  12. Tap Submit (F).
    The Device Settings page appears.
  13. Tap LED Indicator Behaviour (G), select any one of the following options, and then tap Done:
    • Always On: The LEDs on the fan controller are always on.

    • Dim after 5s: The LEDs on the fan controller dim after 5s.

    • Off after 5s: The LEDs on the fan controller turn off after 5s.

  14. Tap LED Indicator Position (H), select any one of the following options, and then tap Done:
    • Position 1

    • Position 2

    • Position 3

    • Position 4

    TIP: For more information about the positioning, tap .
  15. Tap Submit (I).
    Now, you can see the newly added device on the Devices page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?