DUG_Iconic Fan controller_WHP-01

LED indicator settings

You can change the LED indicator behaviour and position settings using the Wiser Home app.

  1. On the Home page, tap All > Iconic Fan Controller.

  2. On the device control panel page, tap Device Settings.

LED indicator mode

You can select the LED indicator behaviour for easy identification of the fan controller status.

Tap LED Indicator Behaviour, select a behaviour (A) from the following options, and then tap Done:

  • Always On: The LEDs on the fan controller are always on.

  • Dim after 5s: The LEDs on the fan controller dim after 5s.

  • Off after 5s: The LEDs on the fan controller turn off after 5s.

For more information on LED during each modes, refer to LED indication.

Position settings

The Fan Controller can be installed in 4 different positions. This feature allows the user/installer to select the position of the low/medium/high speed LEDs to maintain the same sequence across different fan controllers.

Using the app, you can choose the position.

Tap LED Indicator Position, select one of the following options, and then tap Done:

  • Position 1

  • Position 2

  • Position 3

  • Position 4

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?