DUG_Iconic Fan controller_WHP-01

Configuring the device

You can configure the device according to your preference using the Wiser Home app.
  1. On the Home page, tap .
  2. Tap Devices > Appliances > Iconic Fan Controller.

    A

    Device Name: Tap to change the name of the device.

    B

    Location: Tap to assign the Device to any room (such as living room, bedroom, kitchen etc). Refer to changing the device location for more details on how to set the location.

    C

    LED Indicator Behaviour: Tap to set the LED indicator behaviour of the device as per your preference. Refer to LED indicator behaviour for detailed information on each option.

    D

    LED Indicator Position: Tap to set the LED indicator position of the device as per your preference. Refer to LED indicator position for detailed information on each option.

    E

    Identify: Tap to identify the device. The status LED blinks white and connected devices blinks On/Off, upon successful identification of the switch.
    Tap OK when you finish identifying the device.

    F

    Delete: Tap to remove the device from the system.

    NOTE:
    • Removing the device will also reset the fan controller. After reset, the LED turns amber indicating that the fan controller is ready for pairing.

    • If there is a problem while pairing or resetting the switch, refer to resetting the device.

    G

    Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.

    • Good Signal (between 0 & -54dBm)

    • Normal Signal (between -54 & -79dBm)

    • Poor Signal (<-79dBm)

    • No Signal (device is offline)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?