DUG_Iconic Fan controller_WHP-01

LED indication

Pairing the device

User Action

LED Indication

Status

Press and hold the push button for > 8 s.

LED blinks amber.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for a few seconds before turning Off.

Resetting the device

User Action

LED Indication

Status

Short press the push button 3 times and hold it down once for > 10 s.

LED blinks red once per second.

The device is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks amber indicating that it is ready for pairing.

LED indicator mode

LED indicator mode

Speed

LEDs

Timeout

Locator*

Always On

Low

LED1

0

No

Medum

LED1 and LED2

High

LED1, LED2, and LED3

Off

LED1, LED2, LED3, and LED4

Act as a Locator

Low

LED1

5 s

Yes

Medum

LED1 and LED2

High

LED1, LED2, and LED3

Off

LED1, LED2, LED3, and LED4

On with Timeout

Low

LED1

5 s

No

Medum

LED1 and LED2

High

LED1, LED2, and LED3

Off

LED1, LED2, LED3, and LED4

*Glows all four LEDs in lesser brightness after the time out

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?