DUG_Iconic Fan controller_WHP-01

Setting up a schedule

The fan controller can be fully controlled by schedule. Once the schedule is set, the fan controller operates at a given time.
To create a schedule:
  1. From the Home page, navigate to Automations page.
  2. On the Automations page, tap Schedules.
    TIP: To access the schedules page, you can also select All > Fan Controller > Create or assign a schedule.
  3. On the bottom right corner of the screen, tap +.
  4. Enter the name of the schedule in the name field (A).
  5. From the TYPE menu, select Fan Controllers (B) and find the Ceiling Fan (C).
  6. Tap Create (D) to setup events.
  7. From the Events page, tap + to add events such as STATE (Fan speed Off/Low/Medium/High) (E) and WHEN (Sunrise/Sunset or specific time range) (F).
  8. Tap Set (G) to save the schedule.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?