DUG_Iconic Fan controller_WHP-01

Switching On/Off the device manually

You can turn on/off or control the fan speed manually.

Shortly press the push button to turn on the fan at a low speed, then press it again to change the speed to medium and then again to high.

Press and hold the push-button for 1 s to turn off the fan.
You can also turn off the fan by short pressing the push button once when it is at high speed.

TIP: You can change LED behaviour in Wiser Home app setting.

Refer LED indication setting.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?