DUG_Iconic Fan controller_WHP-01

Switching On/Off the device using the app

You can switch on/off the device using the Wiser Home app.
  1. On the Home page, tap All and then find a device.
  2. Tap (A) to turn on/off the fan controller.
    TIP: You can also turn on/off (B) the fan from the control panel and adjust the speed by tapping Low/Medium/High (C).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?