DUG_Wiser 6A — 2 Way Connected Switch 1M-00

About this product

6 A – 2 Way Connected Switch 1M(hereinafter referred to as switch) is used to operate resistive, inductive or capacitive loads.

Control options

App control: To control the switch through the Wiser app.

Direct operation: The switch can always be controlled manually.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.