DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Resetting the device

You can reset the device to factory default manually.

Short-press the power push button 14 times (<10 s).
The LED blinks green after 10 sThe LED blinks green after 10 s.All LED’s blinks green after 10 s.

NOTE: After reset, the device is ready for pairing.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.