DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Editing an action

To edit an action:

  1. On the Automation screen, tap Quick.
  2. On the top-right screen, tap .
    The Edit Actions List screen appears.
  3. On the Edit Actions List screen, tap the action you want to edit.
    TIP: If you want the same action, tap the hand symbol, it will copy the same action and add it to the Edit Actions List.
  4. You can perform the following changes:
    • Change the icon.

    • Rename the action.

    • Add a device or an action.

    • Remove a device or an action.

    • Change the time delay (Only for Add a Sequence).

  5. Once all the edits are done, tap Update.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.