DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Creating a new room

You can create a new room using the Wiser app.

To create a new room:

  1. On the Home screen, tap Devices > Rooms.
  2. Tap + to create a new room.
    The Add Room screen appears.
  3. Enter the room name in the name field (A).
  4. Tap Add Room (B).
    The new room is added to the Rooms tab.
    TIP: If no devices are assigned to the room, tap room > > + to add a device from the Add Device screen. If a device is already added, you can tap + to add another device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.