DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Room Status

You can see the room status using the Wiser app.
  1. On the Home screen, tap Devices > Rooms.

The following screen displays the status of various rooms.

A

3 ON

Displays the number of devices that are ON in the room.

B

All off

Displays that all devices are turned OFF in the room.

C

No devices

Displays that no devices are added to the room.

D

Offline

Displays that all devices in the room are offline.

E

— — —

Displays that no operational devices are added to the room.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.