DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Creating a schedule

The device can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.

You can create separate schedules for each connected device by following the steps below.

To create a schedule:

  1. On the Devices page, tap Devices.
  2. Select the device for which you want to create a schedule.
  3. Tap Schedule.
  4. On the Schedule page, tap Schedule tab, and tap + to create a schedule.
    The Add Schedule page appears.
  5. Add the following details when creating a schedule:
    • Name (A): Enter a name for the schedule.

    • ON Time (B): Select the desired start time.

    • OFF Time (C): Select the desired end time.

    • Weekdays (D): Select the schedule for weekdays.

    • Weekend (E): Select the schedule for weekends.

    • Only once (F): Select the schedule for weekends.

    NOTE: If you want to create a schedule on a specific day, select the day you want to schedule.
  6. Tap Save (G).
    The new schedule is added to the Schedule page.
  7. Tap Delete (H) and then select Ok to delete a schedule.
  8. Tap the toggle button (I) to turn on/off the schedule.
    NOTE:
    • You can edit the On Time, Off Time, and Days whenever you want to make changes.

    • After editing the schedule, tap Update.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.