DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Deleting a trigger

To delete a trigger:

  1. On the Automation screen, tap Trigger.
  2. On the top-right screen, tap to remove a trigger.
    The Edit Actions List screen appears.
  3. On the Edit Actions List page, tap the remove button that is next to the trigger, and then tap Delete to remove it.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.