DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Pairing the device

Using the Wiser app, you can pair your connected curtain controller puck with the Wiser Hub to access and control the shutter.
To pair the device:
IMPORTANT: Before pairing the device, connect your mobile to the home Wi-Fi network.
  1. On the Home screen, tap Devices.
    The Device Management screen appears.
  2. Tap Devices > +.
    The Add Device screen appears.
  3. Tap Preferred > Without Hub > 2 Way Switch (A).
  4. Add the following Device Information:
    • Enter Device Name (B): Add the device name.

    • Assign Existing Room (C): Select an existing room.

    NOTE: If your room is not in the existing room, create a new one.
    • Add New Room (D): Create a new room.

  5. Press the push button 4 times in 10 s.
    The LED indicator rapidly blinks green.
    NOTE: If the LED does not blink, reset the device and attempt pairing again. For instructions on resetting the device, refer to Resetting the device.
  6. Tap Next.
    NOTE: To begin scanning for devices, make sure to enable Bluetooth permissions.
  7. Tap MAC ID (E).
    NOTE: If you are unable to find the device, tap Rescan (F).
  8. Tap Select Wi-Fi (G) and choose Wi-Fi network.
  9. Enter the Wi-Fi password in the password field.
    NOTE: After entering the password, the Connect (H) button will be enabled.
  10. Tap Connect (H). The progress of the device addition will be displayed.
    Now, you can see the newly added device on the Devices page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.