DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Switching On/Off the device manually

You can switch on/off the device manually. The device will provide power to the electrical appliance connected to it.
Short press the push button on the device once to switch on/off the 6A 2 Way Connected Switch.
NOTE: It is normal for the front surface of this product to become warm in use.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.