DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Energy

The energy page displays the device’s total energy consumption in kilowatt-hours (kWh) over several time intervals such as the hour, day, last 7 days, month, and year. This allows you to track and analyze your energy usage patterns over a specific time.
  1. On the Home page, tap Devices.
  2. Select the device.
  3. On the bottom of the screen, tap Energy (A).
    The Energy page appears.
  4. The energy consumption displays the following options:
    • Live (B): Display the Voltage, Current, Total Energy, Power, Apparent Power, and Power Factor.

    • Day (C): Displays the total consumption for the selected day. You can select the day by tapping the day.

    • Month (D): Displays the total consumption for the selected month. You can select the desired month by tapping the month.

    • Year (E): Displays the total consumption for the selected year. You can select the year by tapping the year.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.