DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Notifications

The app will send notifications related to your device when you enable the notification button.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. Tap Settings > Notification.
  4. Tap the Device Online/Offline notifications (A) toggle button to receive notification whether the device has power supply or notNotify Me (B) toggle button to receive notifications.
  5. Tap the Standby Notification (C) toggle button to receive notifications when a device is consuming less than the standby value.
    NOTE: The maximum value you can set is 200 watt.
  6. Tap the Usage Reminder (D) toggle button to receive notifications when a device is on for more than the set time.
    NOTE: You can set the time by tapping the time.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.