DUG_Wiser 6A — 2 Way Connected Switch 1M-00

Creating an Automation for Trigger

Automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app, you can create automation based on your needs.
  1. On the Automation screen, tap Trigger.
  2. Tap + (A) to create an automation.
  3. Tap Add Trigger (B).
    The Select Trigger screen appears.
  4. Select a trigger option from the following list on the Select Trigger screen:
    • Time (D)

    • Location (E)

    • Device (F)

    • Power (G)

    • Weather (H)

    1. Tap Time (D), select any one of the following options and then tap Save.:
      • Any time: Set for any time.

      • At Specific time: Set for a specific time.

      • At in between time: Set for in between time.

      • Perform only once: Set for only once.

    2. Tap Location (E), select any one of the following options:
      • Arriving location: Select arriving location.

      • Departing location: Select a departing location.

      NOTE: Mobile location should turn on.
    3. Tap Device (F) and select a device from the list.
    4. Tap Power (G) and select an option from the following list:
      • EMD B

      • EMD R

      • EMD Y

      • Schneider

      NOTE: This option is only available when the EMD or Meter device is installed in your Home or location.
    5. Tap Weather (H) and select an option from the following list:
      • Outside Temperatures: Select the temperature to trigger an action.

      • Outside Humidity: Select the humidity level.

      • When Sunrises: Select when sunrises.

      • When Sunsets: Select when sunsets.

  5. Tap Add Device (C) and select either a device or an action:
    • Devices (J): Select a device from the list and set the device status (e.g., ON/OFF, delay). Then, tap Done.

    • Control actions (K): Tap View all actions, select an action from the list, and set the action status. Then, tap Save.

    TIP: Tap and enter your device name to find it.
  6. Repeat steps 5 to add more than one device or an action.
  7. Enter the Action Name.
  8. Tap Icon and select the icon from the list.
  9. Tap Notification and enable the toggle button for the following options:
    • Show timeline: Displays the total power consumption.

    • Push notifications: Receives the notifications.

  10. Once all the actions are set, tap Save.
    You can see the newly created automation on the Trigger tab. Tap the toggle button to enable or disable the automation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.