DUG_Wiser 6A — 2 Way Connected Switch 1M-00

LED indication

Pairing and AP Mode

User Action

LED Indication

Status

Press the push-button 4 times in 10 s.

Blinking green rapidly.

Pairing mode is active for 3 minutes. When pairing is completed, the LED will display a solid green if a device is ON; otherwise, no LED will be displayed.

Press the push-button 8 times in 10 s to change the Wi-Fi access point mode.

Blinking green rapidly.

Change AP mode is active for 3 minutes. When the change AP is completed, the LED will display solid green if a device is ON; otherwise, no LED will be displayed.

Resetting

User Action

LED Indication

Status

Press the push-button 14 times in 10 s.

Blinking green rapidly.

Pairing mode is active for 3 minutes. When pairing is completed, the LED will display a solid green if a device is ON; otherwise, no LED will be displayed.

LED Indicator Mode

LED Indicator Mode

LED Indication

Load Off

No LED

Load On

Solid green

Device disconnected from the router after pairing

No LED

OTA update

No LED

Reset state / Not paired / Not added

No LED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.