DUG_Energy Monitoring Device Three Phase-01

About This Product

ENMOD3P is a three phase, three channel communication Energy Monitoring Device (EMD). Its ability to connect to Wi-Fi without the need for a gateway enables convenient circuit monitoring.

EMD is also suitable for monitoring for a three phase system of:

  • Solar energy monitoring,

  • Diesel Generator (DG) energy monitoring,

  • Machinery or equipment monitoring,

  • Individual circuit monitoring.

The accuracy of the product is class 2. It can be mounted on the DIN rail along with the protection devices in the distribution board or can be wall mounted using the provided accessory. One of the key feature of the EMD is its support for data availability through the Wiser app for iOS and Android, which allows you to access and monitor the data for the connected circuits. Multiple EMD can be used for different circuits and aggregated to have a consolidated data. It also offers RS–485 port for wired connection and external antenna for better connectivity.

The key features of ENMOD3P are:

  • It accurately measures real-time values of:

    • Voltage

    • Current

    • Power factor

    • Active power

    • Apparent power

    • Reactive power

    • Active energy

    • Apparent energy

    • Reactive energy

  • Through the Wiser application for iOS and Android, ENMOD3P provides:

    • Support for data availability

    • Overall energy management

NOTE:
  • Current Transformers (CTs) and the ENMOD3P device are not interchangeable with other ENMOD3P devices and CTs.

  • Check MAC ID marking on the product and CT for confirmation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?