DUG_Energy Monitoring Device Three Phase-01

Removing the Device

Using the Wiser app, you can remove a device from the device list.
  1. On the Home tab (A), tap Devices (B).
    The Device Management page appears.
  2. Tap next to Device Management (C).
    The Edit Devices page (D) appears.
  3. Tap to the Delete button (E) next to device and tap Confirm to save the choice.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to Resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?